FB#.SINGLETURNBITS
Description
Number of single turn bits used for BiSS
"Bi-directional Serial Synchronous interface"
An open-source communication protocol for feedback devices. With BiSS, all of the computation for interpolation in regard to position occurs on the ASIC directly in the encoder rotary encoders. Feedback data sheet should specify the number required.
Context
Only used for when FB#.MECHTYPE is linear and identified feedback is BiSS. See Feedback Devices.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
single turn bits |
|
Range |
1 to 32 |
|
Default Value |
19 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.